cancel
Showing results for 
Search instead for 
Did you mean: 

I am working on VND5T100AJ-E for HSD, wondering if any control option driver available from ST, or any one has control logic for overload, open-load in off-state actions?

JWang.38
Associate
 
1 REPLY 1
MBONA.1
ST Employee

The device is a simple switch with a diagnostic pin that gives us feedback on overload and open-load and general device condition.
There is no internal logic capable of triggering actions  in case of overload or open-load. except thermal protection. In case of thermal shutdown is triggered, the device can be programmed as auto-restart or latch-off, depending on FR_Stby status and according to "Table 11. Truth table".
All action have to be controlled either with a microcontroller or at application level, usually with external components.