Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

is an output control switch of LED2001 practical

Dear Support/Expert I have a question about LED2001, is it practical to apply a relay to switch the LED off, but keep the DIM enabled.  as in the schematic. if K21 is off, it will cut the current off of the output, but the DIM pin of the LED2001 is s...

Dsun21_0-1720714726258.png
Dsun.21 by Associate II
  • 2079 Views
  • 3 replies
  • 1 kudos

SPV1040 not working as expected

I have this design using SPV1040 It uses SM102K06L solar panels, that have Vmpp = 3.35V, Impp = 0.406 A (Pmpp = 1.36W). The output must charge a 4.2 Li-Ion battery. At direct sunlight with one panel, I am measuring 0.39 A, and 1.81 V (voltage measure...

doragasu by Associate
  • 993 Views
  • 0 replies
  • 0 kudos

Resolved! Follow up Case: 00206525

Dear Support, This is Lindy From NKG GQA team and I would like to follow up on Case No. 00206525. We would like to understand if there is any update regarding the Smelter CID002645 and CID003470 removal as requested by WD. Could you please provide th...

Lindy_0-1720000344989.png
Lindy by Associate
  • 1525 Views
  • 3 replies
  • 0 kudos

VIPER26LD 310VDC to 15VDC Converter Design Issue

Hi,  I have used following STM reference design for the buck converter. When I power the circuit output doesn't stabilize. What am I missing?   This is from. STEVAL-IHM023V3 Here is my design.   Here is the layout   Best Regards.  

Screenshot 2024-07-10 at 16.18.33.png Screenshot 2024-07-10 at 16.19.08.png Screenshot 2024-07-10 at 16.20.17.png
AAdin.1 by Associate II
  • 2817 Views
  • 5 replies
  • 0 kudos

Electronic speed controller for Drones

I'm designing an ESC for a drone. I found STM's UM2197 design document. I have a question why this DC link capacitor design uses 2 Capacitors in parallel (P/N 35ZLH330MEFC10X12.5) of Rubycon.This capacitor has the following parameters: Ripple Current...

Thanh_0-1715661341872.png
Thanh by Associate
  • 1350 Views
  • 1 replies
  • 0 kudos

Resolved! Minimizing Current Consumption in High Voltage Divider Circuit

Hello everyone,I'm working on a circuit for monitoring the bias voltage of a GM tube, which requires a high voltage of 100V. I am currently using a OA1NP22C op-amp configured as a unity-gain buffer to read the divided voltage. To minimize current con...

Zaim01 by Associate III
  • 11214 Views
  • 29 replies
  • 7 kudos

EVAL-L9963E-MCU firmware & drivers

I am a master's student and working on BMS and I want to use EVAL-L9963E-MCU evaluation board for my research work. But I am not sure whether the firmware or driver for this evaluation board is available in the ST website. Please help me with this in...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.