Skip to main content
RhSilicon
Lead
July 31, 2023
Question

"Not recommended for new designs" should be on the first page. (L9963)

  • July 31, 2023
  • 6 replies
  • 3611 views

If the device is obsolete, it should be easy for new users to identify this.

L9963.png

This topic has been closed for replies.

6 replies

RhSilicon
RhSiliconAuthor
Lead
July 31, 2023

OBSOLETE.png

OBSOLETE_table.png

RhSilicon
RhSiliconAuthor
Lead
July 31, 2023

OBSOLETE2.png

 

OBSOLETE3.png

TDK
July 31, 2023

Isn't it right there next to the part number? Where do you want it to be instead?

TDK_0-1690810346628.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
July 31, 2023

Presumably if you bump up a level it will list all parts in the same category, and with status too.

Is the problem here it doesn't list drop-in alternatives, or the font is the wrong colour or insufficiently large?

The part is not "obsolete", they are just are at or near capacity planning for the device, and the economics don't drive expansion or extension of those plans. Perhaps they'd prefer you'd pick something with better margin or yield. Plan accordingly..

It's been my experience that vendors don't really want or need to disclose their reasoning, it's their business to know what they do and do not want to make moving forward. Remember companies like Apple are likely underwriting particular parts, so unless you have a large check book to do the same, the focus is going to be on the products that the "Big Company" wants delivered.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RhSilicon
RhSiliconAuthor
Lead
July 31, 2023

The information is coded, it doesn't hurt to put the text in full instead of abbreviating it.

Elena BRAMBILLA
ST Employee
October 25, 2023

Hello,  you are right. In any case the board is not obsolete: it's only Not Recommended for New Design because linked to L9963 that is NRND as well.

If interested you need to refer to the the product L9963E and related boad EVAL-L9963E.

regards.

Elena