Dear Divyansh12, there is something strange on this behavior. To support you we need to have a schematic and more information. Waiting for your feedback. BR
Dear rkager, you can refer at this link for your request:User manual - UM1922 - VIPower® M0-7 standard high-side drivers hardware design guideParalleling of devices can help you.BR
ciao Dazai, you're right! the only difference between the VN9D5D20FN and VN9D5D20F is the presence of the reverse battery through self-turn on (in the VN9D5D20F). This feature is intended to avoid high power dissipation during reverse battery polarit...
Hi, the current limit reported in the datasheet is linked to inrush (transient) condition, not steady state.The VN7050AS is housed in a SO-8 package and the maximum DC current depends on PCB copper area on which the device is soldered. Looking at the...
The device is a simple switch with a diagnostic pin that gives us feedback on overload and open-load and general device condition.There is no internal logic capable of triggering actions in case of overload or open-load. except thermal protection. I...