2017-03-27 9:51 AM - last edited on 2025-02-11 11:51 PM by Peter BENSCH
Posted on March 27, 2017 at 18:51
I'm using STM32F303 which operates on 3.3V
how can I communicate with the L9823 SPI which runs via 5V?
thank you
Solved! Go to Solution.
2025-02-12 12:08 AM
Unfortunately, the question ended up in the wrong subforum a long time ago, so the answer will no longer help the TO. For the sake of completeness and in case someone stumbles across the same question:
To bring this H level to the value required by the E-L9823, a voltage translator or level shifter is necessary. A simple stage with open-drain or open-collector is not sufficient as a level shifter, as this does not achieve the required transmission frequency due to the passive pull-up.
Regards
/Peter
2025-02-12 12:08 AM
Unfortunately, the question ended up in the wrong subforum a long time ago, so the answer will no longer help the TO. For the sake of completeness and in case someone stumbles across the same question:
To bring this H level to the value required by the E-L9823, a voltage translator or level shifter is necessary. A simple stage with open-drain or open-collector is not sufficient as a level shifter, as this does not achieve the required transmission frequency due to the passive pull-up.
Regards
/Peter