2019-03-12 1:09 AM
Hello,sir/mam
We have developed the schematic as per the reference of the STREF-SCS001V1 Board.
I know the STUSB4500 requires PD enable charger as its source so we have taken PD enabled adapter.
I have been using STM32F072 EVM board to detect the STUSB4500 IC .
I have imported the "NUCLEO_F072RB_STUSB_UART_NVM_config_1.04.bin" File in the STM32F072.
I took out the connection(SCL,SDA) from my PCB ,Also connected the PD enabled Adapter and combined my Circuit and STM32F072 Ground.
After uploading the .bin file when i am opening the GUI its Showing Error STUSB4500 not detected.My LD2 green LED works fine on STM32F072 EVM board.
I am attaching you my schematic please verify and suggest solution regarding this.
Your help would be appreciated.So waiting for your Quick response.
STUSB4500 Type c schematic
2019-03-19 3:35 PM
Hi,
Please make sure you have pull-ups, because I didn't see them on your schematic.
Please use the latest version of the GUI (v1.0.8 or later) :
2022-09-21 12:14 AM
Hi,
I am looking for NUCLEO_F072RB_STUSB_UART_NVM_config_1.04.bin file for flash the Nucleo-64 board. Where I can find it?
I would like to change a STUSB4500 cPD config and it seems that without this tool, is not possible as the flash NVM protocol is not available on any ST document.
Thank in advance
Thierry