2022-08-30 7:15 AM
Query above is straight forward. - Deadtime implementation options for Half Bridge config.
Deadtime is to "wait for one FET to switch off" b4 turning on the other FET in the half bridge. This is to prevent shoot thru for the Power supply via the Half bridge..
Solved! Go to Solution.
2022-09-21 7:36 AM
Hello @Benji and welcome to the ST Community.
The STGAP2SICS is a single gate driver there is no the possibility to set a dead time (DT).
You can generate the desired DT with the external PWM coming from a MCU and applying them to the input signals of STGAP2SICS.
2022-09-21 7:36 AM
Hello @Benji and welcome to the ST Community.
The STGAP2SICS is a single gate driver there is no the possibility to set a dead time (DT).
You can generate the desired DT with the external PWM coming from a MCU and applying them to the input signals of STGAP2SICS.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.