2020-01-27 3:37 AM
I am using X-NUCLEO-IHM06A1 Board with Nucleo-F401RE to control the acceleration, set target speed, home position and target position of stepper motor in my program code. I already referred user manual as well as datasheet which is available but I am not getting any information for writing code. I want to control all these parameters by program only.
please send me all information regarding this issues as well as sample code through stm-cube max if possible.
Best Regard
Ravi
2020-01-28 5:51 AM
Hello,
several there are options:
Regards, Cristiana