cancel
Showing results for 
Search instead for 
Did you mean: 

Greetings all, I am working with the gate driver STDRIVE101 to drive a BLDC motor. For the current sensing opamps, the value of the filter capacitor was calculated based on the cut-off frequency, my question is, does this cutoff frequency depend on Fsw?

HIbra.1
Associate

Fsw is the switching frequency of the Mosfets, i am asking if this value should be considered when calculating the filter capacitor value or not

2 REPLIES 2
Cristiana SCARAMEL
ST Employee

Hello @HIbra.1​ and welcome to the ST Community.

Are you using our EVALSTDRIVE101 demonstration board or a custom board?

In the second case, could you share the schematic?

To set the cut-off filter frequency you have to consider two points:

  • the target is to filter ringing on PWM rising edges
  • the filtering effect slows down the PWM edge (therefore waiting more time to sample)

You must find a tradeoff between these aspects.

In general a cut-off frequency of the order of 1 MHz can be enough.

Moreover take into account that the OpAmp has its own limited bandwidth that acts as filter itself

(e.g. GBWP = 10 MHz, setting a gain of 10 --> BW = 1 MHz).

I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".

If you feel a post has answered your question, please click "Accept as Solution"

Hello @HIbra.1​ there are updates from you?

If you feel a post has answered your question, please click "Accept as Solution"