2022-10-31 01:29 AM
Fsw is the switching frequency of the Mosfets, i am asking if this value should be considered when calculating the filter capacitor value or not
2022-11-03 08:11 AM
Hello @HIbra.1 and welcome to the ST Community.
Are you using our EVALSTDRIVE101 demonstration board or a custom board?
In the second case, could you share the schematic?
To set the cut-off filter frequency you have to consider two points:
You must find a tradeoff between these aspects.
In general a cut-off frequency of the order of 1 MHz can be enough.
Moreover take into account that the OpAmp has its own limited bandwidth that acts as filter itself
(e.g. GBWP = 10 MHz, setting a gain of 10 --> BW = 1 MHz).
I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".
2022-11-24 12:41 AM
Hello @HIbra.1 there are updates from you?