2019-05-28 07:48 PM
Hi
I would like to make battery charger by applying EVLSTNRG-1KW
** BATTERY CHARGER SPECIFICATIONS
Total capacity – 3 [KW]
input voltage – 100 ~ 420 [VDC] (input from solar panel)
3. output voltage – max 430 [VDC] (battery charger voltage)
** Question
1. In the Application note(AN4689) I saw that it was possible to scale up to 3kW (400V maximum output voltage).
-> Is it possible to have maximum output voltage up to 430VDC?
2. If yes, is it possible to apply the EVLSTNRG-3KW to a battery charger?
3. Can I get the 3KW scaled up data(application note, diagram, etc)?
4. Is software and programs of the STNRG388A control board provided by the ST Company?
5. If I order EVLSTNRG-3KW products, how about the Delivery date?
- (about quantity 3 ea, KOREA)
Thank you
Have a nice day.
(** I would appreciate tour reply in my email.(marutop1@naver.com))
2019-05-29 02:44 AM
I think this is a question for your local FAE, not the forum