cancel
Showing results for 
Search instead for 
Did you mean: 

EVLSTNRG - 1KW Product Inquiries

KYOON
Associate

Hi

I would like to make battery charger by applying EVLSTNRG-1KW

 

** BATTERY CHARGER SPECIFICATIONS

Total capacity – 3 [KW]

input voltage – 100 ~ 420 [VDC] (input from solar panel)

3. output voltage – max 430 [VDC] (battery charger voltage)

 

** Question

1. In the Application note(AN4689) I saw that it was possible to scale up to 3kW (400V maximum output voltage).

-> Is it possible to have maximum output voltage up to 430VDC?

2. If yes, is it possible to apply the EVLSTNRG-3KW to a battery charger?

3. Can I get the 3KW scaled up data(application note, diagram, etc)?

4. Is software and programs of the STNRG388A control board provided by the ST Company?

5. If I order EVLSTNRG-3KW products, how about the Delivery date?

- (about quantity 3 ea, KOREA)

Thank you

Have a nice day.

(** I would appreciate tour reply in my email.(marutop1@naver.com))

1 REPLY 1
MikeDB
Lead

I think this is a question for your local FAE, not the forum