cancel
Showing results for 
Search instead for 
Did you mean: 

Custom WPT RX based on STWLC98JR

dreamscat4er
Associate

Hello!

I am new to circuit design so please treat me patiently :relieved_face:

I am building a receiver circuit based on STWLC98 and following the design guides from STEVAL-WLC98RX wireless power receiver evaluation board manual. My question is what tool can I use to test the circuit without assembling it? I worked with LTspice XVII before, but it does not have all the necessary components. Maybe there is a simmilar tool for STM MPU?

Thank you for any useful reference!

4 REPLIES 4
Didier HERROUIN
ST Employee

Dear customer,

ST has decided to reduce its portfolio to the most successful devices.

Unfortunately, STWLC98 is not part of this portfolio and it is going to be stopped.

Sorry for the inconvenience,

Didier H.

Dear Didier,
How about STWLC99JR and STWBC2-HP? Also, can you advise the tool for circuit testing similar to LTspice?

Hello,

STWBC2-HP continues, but STWLC99 is stopped.

For Rx part, STWLC38 is available (up to 15W) and a new product should be released this year up to 30W.

For Tx, STWBC86 can deliver up 5W and STWBC2-HP covers the whole range (even up to 100W).

BR,

Didier 

 

Thank you for the information!