ST72F324J6 stack problem?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-04-19 3:27 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-04-18 10:13 PM
Hi, I have a strange problem that a cant solve. I use Cosmic compiler, STVD7 with EMU3.
For my application I use short stack memory model. It compiles and links fine, but in run-time it crash sometimes. In main routine I only do this: room_temp= ((float) int_room_temp/1023)*110 - 30; In a timer interrupt I use printf to print values to LCD. The calculation of room_temp is ok as long as not printf is used in interrupt routine. But after an interrupt with use of printf the value of room_temp is totaly wrong. I think it is something wrong with the memory (stack) handling but I cant figure out what happens. Any ideas? Thank you. Map file says: -------- Segments -------- start 00008000 end 0000bd77 length 15735 segment .text start 0000bd80 end 0000c272 length 1266 segment .const start 00000080 end 00000081 length 1 segment .bsct, initialized start 0000bd7f end 0000bd80 length 1 segment .bsct, from start 00000081 end 000000e0 length 95 segment .ubsct start 000000e0 end 000000e0 length 0 segment .share start 00000200 end 00000200 length 0 segment .data start 00000200 end 00000200 length 0 segment .bss start 00000000 end 00005726 length 22310 segment .debug start 0000ffe0 end 00010000 length 32 segment .const start 0000bd77 end 0000bd7f length 8 segment .init ----------- Stack usage ----------- Debug\adc.o: _ADC_Filter 7 (7) _ReadADC 4 (4) _ReadADC_32Avg 15 (8) Debug\initregs.o: _InitRegs 2 (2) Debug\interrupt_vector.o: _NonHandledInterrupt > 5 (5) Debug\lcd16203.o: _LCD_delay 4 (4) _LCD_off > 16 (2) _LCD_on > 16 (2) _LCD_prog_char 20 (6) _LCD_setup 22 (2) _LED_off 2 (2) _LED_on 2 (2) _PutOutData 14 (2) _blink_off 16 (2) _blink_on 16 (2) _clrscr 16 (2) _putchar 17 (3) _setcur 17 (3) Debug\lcd_menu_handle.o: _RTCInterrupt > 198 (18) _init_menu 180 (2) Debug\main.o: _get_PLC_signal > 17 (2) _get_alarms > 9 (6) _get_temperatures > 8 (2) _main > 14 (2) _regulate > 16 (10) Debug\spi_master.o: _Init_SPI_Master 2 (2) _SPI_Transfer 9 (5) _delay 4 (4) _eeprom_read 12 (3) _eeprom_write 13 (4) _set_external_outputs > 14 (5) _set_external_port 12 (3) Debug\taco_control.o: _PB0_Interrupt > 5 (5) _fan_alarm_handle 2 (2) D:\Program\COSMIC\CXST7_16K\LIB\libfs.st7: __addexp > 7 (7) __poly > 11 (11) __unpack 2 (2) __norm 59 (29) L11__cvtup 8 (6) L31__putbuf 26 (9) L7__gnum 19 (16) __print 162 (51) __dtento 30 (20) __dtoe 89 (30) __dtof 91 (32) __dtog 111 (20) _printf 178 (16) __round 7 (7) D:\Program\COSMIC\CXST7_16K\LIB\libis.st7: __udiv 6 (6) __uldiv 6 (6) __itob 22 (16) __ltob 24 (18) _memchr 5 (5) _strlen 2 (2) _toupper 2 (2) Stack size: 215- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-04-18 10:43 PM
Hi.
First and easiest what i would do in such case is to start debugger, before starting programm fill whole stack with 0xff or 0xa5 or whatever, start program, wait for a some time, stop it and check your stack. so, u can see how much of stack was used. of course, if programm crashes u can not get access to stack. by this way u can more or less evaluate the use of stack. repeat it for several times to get ''the worst'' use of stack.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-04-18 11:04 PM
Thanks for reply.
I have done that and the worst case seems to be stack goes from 0x1FF to 0x166. That should be ok? I have also tried to use static memory models. When using memory long I get error ''segment .share size overflow (64)'' from linker.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-04-18 11:34 PM
Well, u can try long stack as well, but i am not sure that it will help. It looks like your bug. Try to disable watchdog.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-04-19 2:43 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-04-19 3:01 AM
Thanks alot!
It seems that the error only occurs when printing float values in the interrupt routine. I will follow your advice, I understand this is not the best for a small micro, but still I wonder why it dont work when all memory handle seems ok. BR Bood- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-04-19 3:12 AM
Quote:
..still I wonder why it dont work when all memory handle seems ok.
printf uses resources that are not saved by default when entering the interrupt routine; you could force the compiler to save all that stuff (notably, the LREG), but, as using printf under interrups is wrong anyway (no predictable execution time), you'd better remove it altogether. Regards, Luca- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-04-19 3:27 AM
OK, thank you again.
I have removed it and it seems to be running fine now.