Posted on May 17, 2011 at 10:19Hello. Looking code example of bldc sensor control from st7 i was a little bit confused. In mtc.c file, MTC_StartMotor function i found following code : // Init of MTC peripheral hardware registers used modified durin...
Posted on May 17, 2011 at 10:19Hello. I want to use Safe oscillator function to control my oscillator state. It means i have to enable PLL. Enabling PLL gives Fclk=16MHz (ST7MC datasheet, page 23, figure 11) having 8MHz frequency at the input of PLL...
Posted on May 17, 2011 at 10:19Hi. Torque is one of the basics of physics. Books describe it perfectly. As far as you have st7mc2 read this datasheet (http://www.st.com/stonline/books/pdf/docs/9721.pdf), especially 9.6 section. Don't worry if u will...
Posted on May 17, 2011 at 10:19I understood that there are 6 steps, cause the motor has 3 windings. Am I right ? >> Yes, you 'r. Number of steps depends on number of windings, but could be also 12, 24 ... (I have implemented 12 steps, 24 -- may be i...
Posted on May 17, 2011 at 10:19Hi. I will share with you my experience. I am only beginer as well. I deal with motors since half of year and at most cases all information i get from st ap. notes. If you will read carefully you will get answers on mo...