2005-07-28 09:11 PM
.s files in USB Library are not compilable with IAR EWARM
2005-07-27 09:51 PM
Hello,
I am using IAR EWARM compiler for building USB Library Demo project. I found that the .s files in the library are not compilable with this compiler. I think there is some directives etc. which are not supported. Does anybody have rectified these files for being able to be compiled by this compiler ?? Regards, Chander2005-07-28 07:23 PM
Thanx Zouh, I am able to compile these files now. But I am also getting a lot of errors in C files also. Could you send me the C files also if you have already modified these files.
Thanx in advance. [ This message was edited by: chander on 29-07-2005 07:54 ]2005-07-28 09:11 PM
Gr8. I am able to build the executable now.
Thanx for the help.