cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with the register XIR0SEL

simeon
Associate
Posted on July 29, 2005 at 04:50

Problems with the register XIR0SEL

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
simeon
Associate
Posted on July 26, 2005 at 11:26

Hello,

I use ST10f276 microcontroller with KEIL compiler and I have some problems with the CAN controller. CAN1 interrupt must be enabled additionaly by the register XIR0SEL.

I do the following:

- CAN-interrupts initialisation:

XPERCON |= 0x401; //XMISCEN=1, CAN1EN=1

SYSCON |= 0x4; //XPEN=1

CAN1_CR = 0x2A; //DAR=1, EIE=1, IE=1

XIR0SET = 0x100; //CAN1 Interrupt Enable=1

XP0IE = TRUE;

- Results:

DEBUG:

OK

RELEASE:

CAN Interrupts are not generated

Why in debug mode everithing is Ok, but in release it doesn't work?

I use the CAN to send with a PDO the content of XIR0SEL and I can observe the communication with a special tool.

I saw that each line changes the content of register XIR0SEL (???):

For example:

XIR0SEL is =0x0700

CAN1_IF1_CM = 0xB7; //IF_WRRD=1, IF_ARB=1, IF_CNTRL=1, IF_TXR_ND=1, IF_DATA_A=1, IF_DATA_B=1

now XIR0SEL is changed to 0x00B7 ???

CAN1_IF1_A2 = (0x350 << 2) | 0xA000; //IF_MSGVAL=1, IF_DIR=1;

and now XIR0SEL is changed to 0xAD3C ???

CAN1_IF1_MC = 2 | IF_EOB;

XIR0SEL is changed to 0x0082 ???

Maybe I'm doing something wrong... Is there anybody who can help me?