Posted on July 18, 2006 at 06:56Hi, Does there exist some application note which tells how to port a RVDK project to IAR EWB project. All of the source code available on the site is based on RVDK. It is almost impossible to port the code on IAR Embe...
Posted on July 29, 2005 at 04:23Thanx Zouh, I am able to compile these files now. But I am also getting a lot of errors in C files also. Could you send me the C files also if you have already modified these files. Thanx in advance. [ This message wa...
Posted on July 28, 2005 at 06:51Hello, I am using IAR EWARM compiler for building USB Library Demo project. I found that the .s files in the library are not compilable with this compiler. I think there is some directives etc. which are not supported...
Posted on June 02, 2005 at 03:26Jackie, The new version of STVP7 will support the ST72F63BK6 device. It will be released in 1 or 2 months. However, if your software is less than 16 K, then you can program the device by selecting BK4. Pls make sure t...