2003-11-12 7:49 AM
PSD Express, relation of files and tools, building from command line
2011-05-17 2:56 AM
PSDSoft is a good tool to get a result within short time but I am a bit confused about the type of files which are produced. Can somebody inform me about which files are the input to which tools and what output files are produced?
I store every source file of a project in a revision control system and it would be nice to know which files are ''original'' data and which are generated or just temporary data. There are a lot of ''exe''-files in the PSD directory. Is it possible to have the complete project built up from the commandline? Michael