Skip to main content
jdaniel
Associate III
November 12, 2003
Question

Flash Merge / Program From Command-Line

  • November 12, 2003
  • 2 replies
  • 670 views
Posted on November 12, 2003 at 14:08

Flash Merge / Program From Command-Line

This topic has been closed for replies.

2 replies

sjo
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:56

To merge do the following:

c:\PSDexpress\utladrm.exe C:\Projects\micro\upsd\dk32dsn2\DK3200_2_p\DK3200_2.ini

and to program:

c:\PSDexpress\FLink.exe -i C:\Projects\micro\upsd\dk32dsn2\DK3200_2_p\DK3200_2.jcf -d OD

I have set up the first as user program 1 in keil options output, the second is setup as the configured Flash Programming tool in utilities.

Regards

sjo
jdaniel
jdanielAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:56

I was wondering if it's possible to pass commmand-line arguments to PSDSoft express for merging firware with a PSDSoft design and/or programming. I have saved the programming options needed for my project, but I'd like to set up a build step in my development environment that allows me to merge my firware with uPSD settings and then download the code. If there is any way to do this (even if it requires the use of something other than PSDSoft), please let me know. Thanks.

Best Regards,

Phaze426