2003-11-17 12:17 AM
programming the ST72F264 Using the ST7 IN DART
2003-11-16 9:19 PM
hi !!
i'm using the ST72F264 DEMO BOARD , the in dart-stx , indart ST7 and the metrowerks as a compiler with the plug in installed. now i'm trying to program my device but with no success, here are my steps maybe you can help me to verify what i do wrong (or did not do and need to do) : 1. i set the MCU i'm using the MCU configuration menu 2. i set the option byte 3. i load with in the indart the *.abs file but i get errors like : gdi-error in indart. debugging with the metrowerks have no problams so far. pleade advise. thanks. adi.2003-11-16 10:07 PM
Are you sure that the selected clock source in the option byte is available in your application ?
2003-11-17 12:17 AM
you are right, the clk source was not configure proper.
thanks