Posted on April 17, 2005 at 09:40Hi !! what is the recommended state of un connected ios ??? input/ output, shall i connected it through a resistor to the gnd ? leave connection open ???
Posted on November 24, 2003 at 13:51yes ,it is written in the datasheet but not under the output compare function section and i just wanted to be sure. thanks.
Posted on November 24, 2003 at 12:01hi ! when i use the output compare function , when i'm writing to the CLR register will it reset the counter ???? thanks. adi
Posted on November 18, 2003 at 13:29 hi ! i'm using the st72264 with the in dart and i encounter jitter which is un acceptional while using output compare function or even the PWM function. i measure time and when the time is over i toggle a...