Hello Community,
I am trying to build a 333V Battery Pack with AEK-MCU-C4MLIT1 as the Master, AEK-ISOSPI Translator and multiple AEK-POW-BMS69EN as slaves in daisy chain configuration. I would like to get the information such as cell voltages, SOC, and Balancing commands from the slave and send it onto the Vehicle CAN Network.
As of now, I have been able to get the cell voltages on the serial terminal from one 48V dummy pack which I have built. And, I have been able to send some dummy data from the AEK-MCU-C4MLIT1 Master CAN 1 Channel and read it with the help of a CAN KVASER Dongle.
Now, When I went for combining these two functionality the project didn't seem to work.
I suspect that maybe the pins which I am using to establish the ISOSPI communication between the Master and the Slave are interfering when I am trying to establish the CAN Communication. But, I tried configuring the pins on the CAN0 channel (Pin 101 as RX and Pin 102 as TX) but I am not seeing anything on the CAN_1_L and CAN_1_H lines on the PCB. I have enabled the MCAN0 channel in the CAN Configuration.
What could I be doing wrong? Is there some example to which I could refer?
I have attached an image of my PIN map and my code.
PS: You can see that I am quite new to learning Embedded programming but I am trying.
My main.c file:
/****************************************************************************
*
* Copyright © 2022 STMicroelectronics - All Rights Reserved
*
* License terms: STMicroelectronics Proprietary in accordance with licensing
*
* THIS SOFTWARE IS DISTRIBUTED "AS IS," AND ALL WARRANTIES ARE DISCLAIMED,
* INCLUDING MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE.
*
* EVALUATION ONLY – NOT FOR USE IN PRODUCTION
*****************************************************************************/
/* Inclusion of the main header files of all the imported components in the
order specified in the application wizard. The file is generated
automatically.*/
#include "components.h"
#include "AEK_POW_BMS63EN_Appl.h"
#include "wkpu_lld_cfg.h"
#include "serial_lld_cfg.h"
#include <stdio.h>
#include <string.h>
#include "can_lld_cfg.h"
volatile uint8_t i_device_disp=0;
void send_temp_data(AEK_POW_BMS63EN_module_t *batteryModule){
CANTxFrame txf_temp;
txf_temp.TYPE = CAN_ID_STD; // Standard CAN frame
txf_temp.ID = 0x615; // CAN ID for Temperature Message
txf_temp.DLC = 8U;
uint16_t temp1 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellTemperatureNTC[0]);
uint16_t temp2 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellTemperatureNTC[3]);
uint16_t temp3 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellTemperatureNTC[6]);
uint16_t temp4 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellTemperatureNTC[9]);
uint16_t temp5 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellTemperatureNTC[12]);
txf_temp.data32[0] = ((temp1 & 0xFFF) << 0) | // 12 bits
((temp2 & 0xFFF) << 12) | // 12 bits
((temp3 & 0xFFF) << 24); // Upper 8 bits of temp3
txf_temp.data32[1] = ((temp3 & 0xFFF) >> 8) | // Lower 4 bits of temp3
((temp4 & 0xFFF) << 4) | // 12 bits
((temp5 & 0xFFF) << 16); // 12 bits
can_lld_transmit(&CAND1, CAN_DEDICATED_TXBUFFER, &txf_temp);
}
void send_cell_voltages_CAN(AEK_POW_BMS63EN_module_t *batteryModule) {
CANTxFrame txf_volt1;
txf_volt1.TYPE = CAN_ID_STD; // Standard CAN frame
txf_volt1.ID = 0x602; // CAN ID
txf_volt1.DLC = 8U; // Data Length (8 bytes per frame)
CANTxFrame txf_volt2;
txf_volt2.TYPE = CAN_ID_STD; // Standard CAN frame
txf_volt2.ID = 0x603; // CAN ID
txf_volt2.DLC = 8U; // Data Length (8 bytes per frame)
// Send 7 cell voltages in the first frame
uint16_t voltage1 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[0] * 100);
uint16_t voltage2 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[1] * 100);
uint16_t voltage3 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[2] * 100);
uint16_t voltage4 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[3] * 100);
uint16_t voltage5 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[4] * 100);
uint16_t voltage6 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[5] * 100);
uint16_t voltage7 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[6] * 100);
//Send remaining 7 cell voltages in the second frame
uint16_t voltage8 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[7] * 100);
uint16_t voltage9 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[8] * 100);
uint16_t voltage10 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[9] * 100);
uint16_t voltage11 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[10] * 100);
uint16_t voltage12 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[11] * 100);
uint16_t voltage13 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[12] * 100);
uint16_t voltage14 = (uint16_t)(batteryModule->AEK_POW_BMS63EN_Pack_CellVoltage[13] * 100);
txf_volt1.data32[0] = ((voltage1 & 0x1FF) << 0) | // 9 bits
((voltage2 & 0x1FF) << 9) | // 9 bits
((voltage3 & 0x1FF) << 18) | // 9 bits
((voltage4 & 0x1FF) << 27);
txf_volt1.data32[1] = ((voltage4 >> 5) & 0x07) | // Remaining 4 bits of voltage[3]
((voltage5 & 0x1FF) << 4) | // 9 bits
((voltage6 & 0x1FF) << 13) | // 9 bits
((voltage7 & 0x1FF) << 22);
txf_volt2.data32[0] = ((voltage8 & 0x1FF) << 0) | // 9 bits
((voltage9 & 0x1FF) << 9) | // 9 bits
((voltage10 & 0x1FF) << 18) | // 9 bits
((voltage11 & 0x1FF) << 27);
txf_volt2.data32[1] = ((voltage11 >> 5) & 0x07) | // Remaining 4 bits of voltage[3]
((voltage12 & 0x1FF) << 4) | // 9 bits
((voltage13 & 0x1FF) << 13) | // 9 bits
((voltage14 & 0x1FF) << 22);
can_lld_transmit(&CAND1, CAN_DEDICATED_TXBUFFER, &txf_volt1);
can_lld_transmit(&CAND1, CAN_DEDICATED_TXBUFFER, &txf_volt2);
}
void main_core0(void) {
char message[11];
AEK_POW_BMS63EN_module_t AEK_POW_BMS63EN_BatteryModule;
uint8_t cell_idx = 0;
/* Enable Interrupts */
irqIsrEnable();
sd_lld_start(&SD5,&serial_config_BMS_serial);
can_lld_start(&CAND1, &can_config_mcanconf);/*MCAN SUB 0 CAN 1*/
/* Application main loop.*/
for ( ; ; ) {
if((osalThreadGetMilliseconds()%500)==0){
AEK_POW_BMS63EN_BatteryModule = AEK_POW_BMS63EN_GetModule(i_device_disp);
send_cell_voltages_CAN(&AEK_POW_BMS63EN_BatteryModule);
//send_temp_data(&AEK_POW_BMS63EN_BatteryModule);
//SOC Elaboration Done
sprintf(message, "DEV:%d \n", (int)(i_device_disp+1));
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing SOC
for(cell_idx = AEK_POW_BMS63EN_CELL1; cell_idx <= AEK_POW_BMS63EN_CELL14; cell_idx ++){
sprintf(message, "S%.2d:%.3d ", cell_idx+1, (int)((AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_SOC[cell_idx]) * 100));
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
sprintf(message," \n");
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Bal
for(cell_idx = AEK_POW_BMS63EN_CELL1; cell_idx <= AEK_POW_BMS63EN_CELL14; cell_idx ++){
sprintf(message, "B%.2d:%.3d ", cell_idx+1, AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_Bal_cmd[cell_idx]);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
sprintf(message," \n");
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Voltage
for(cell_idx = AEK_POW_BMS63EN_CELL1; cell_idx <= AEK_POW_BMS63EN_CELL14; cell_idx ++){
sprintf(message, "V%.2d:%.3f ", cell_idx+1, AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_CellVoltage[cell_idx]);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
sprintf(message," \n");
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
//Printing Current
sprintf(message, "C:%.4f \n", AEK_POW_BMS63EN_BatteryModule.AEK_POW_BMS63EN_Pack_Current);
sd_lld_write(&SD5, (uint8_t *)message, (uint16_t)(sizeof(message)/sizeof(message[0])));
}
}
}
void *sbrk(size_t incr)
{
extern uint8_t __heap_base__;
extern uint8_t __heap_end__;
static uint8_t *p=&__heap_base__;
static uint8_t *newp;
newp = p+ incr;
if(newp> &__heap_end__)
{
return (void*)-1;
}
return p =newp;
}
void int28_irq_cb(WKPUDriver *wkpup)
{
(void)wkpup;
i_device_disp = i_device_disp+1;
if (i_device_disp==AEK_POW_BMS63EN_N_BMS) i_device_disp=0;
}
int main(void) {
componentsInit();
irqIsrEnable();
wkpu_lld_start(&WKPUD1, &wkpu_config_wkpu_cfg);
AEK_POW_BMS63EN_init();
runCore0();
AEK_POW_BMS63EN_Start_Mgn_exec();
while (1) {
}
}