2003-07-15 6:45 AM
2003-07-13 11:01 PM
I own a ST7-MDT-00-EPB2 and I need to modify the supplied user interface to program quite large quantities of the ST7LITE05 MCU.
Simple operators will do the job, placing a device into its socket and then pressing a single button will trigger the programming without any possibility from the operator to change any parameters or code of what they are programming. My question are: Is there any possibility to access the API set of the programmer software in order me to create my own interface. Is this API set available and well documented? I need only de programmer hardware and the low level PC software, I'll do the rest as far as the API is available. Third party programmer manufacturers are welcome also Claudio2003-07-14 11:49 AM
I've written a keystroke program to control the ST7-MDT-00-EPB2 software and afterwards I read the log files.
I would recommend using Spen's flashbash as he provides the software source code which could be modified2003-07-14 6:29 PM
thanks for you help
2003-07-14 11:10 PM
If uou need to program a large quantity of ST7 devices, you can use the SofTec Microsystems MP8011A Gang Programmer. It can program up to 8 devices at time. More info at www.softecmicro.com
--Piero2003-07-14 11:36 PM
Ciao Piero
Does your programmer support serialization?2003-07-15 6:45 AM
Hello,
The MP8011A (gang programmer) doesn't support the serialization. The serialization is available on SofTec Microsystems inDART-ST7 series only (ISP programmer/debugger for ST7). Ciao, --Piero