Posted on November 29, 2006 at 14:26 I am using Keil uVision3 for simulating an STR750 I use the GPIO demo project provided by Keil for this device. After a succesfull compiling and linking I try to start the debugger and I receive the followi...
Posted on July 03, 2005 at 12:55Hi, I enter the ICC mode for the ST7FLITE05 and I see a large current flowing into the RESET pin, about 18 mA for 5 Volts. When I switch the driving output to high impedance in my controller processor(connected to the...
Posted on June 21, 2005 at 10:12Hi, I need to know which the typical current consumption is for the ST7LITE05 when it is running in ICC mode. Internal RC Clock running at 8 MHZ Thanks ..........Claudio
Posted on March 20, 2005 at 08:54I use the ICC interface to download the necessary code to send ST7FLITE to HALT mode. I execute the I/O ports setup and then the instruction HALT. Will the MCU enter the HALT mode? Claudio