Posted on November 17, 2003 at 05:00For ST7 HD-Flash memory- based devices (521, 324, etc), the execution is in real-time only when no breakpoints are set. However, you can set “low-level� breakpoints (and still get real-time execution) by putti...
Posted on November 06, 2003 at 12:06Here is an example of a F264 PRM file: *************************** NAMES END SECTIONS MY_RAM = READ_WRITE 0x0080 TO 0x00FF; MY_ROM = READ_ONLY 0xE000 TO 0xFFDF; PLACEMENT DEFAULT_ROM, ROM_VAR, STRINGS INTO MY_R...
Posted on September 17, 2003 at 05:55Hi, Cosmic IDEAST7 doesn't support inDART debugger directly. But if you want to use the Cosmic compiler with inDART you have to use the ST STVD7 IDE with Cosmic toolchain. Following these steps: 1. Install Cosmic...
Posted on September 10, 2003 at 06:13Brian, If you are using inDART, you can start with the sample provided with the tool. This example configures the A/D peripheral to convert on A/D channel 3 and displays the results on LEDs Bye Piero
Posted on September 08, 2003 at 11:20Hi, If you have any questions about inDART please contact SofTec Microsystems technical support (email: mailto:support@softecmicro.com) SofTec is ready to help you!