Posted on July 14, 2003 at 20:49I've written a keystroke program to control the ST7-MDT-00-EPB2 software and afterwards I read the log files. I would recommend using Spen's flashbash as he provides the software source code which could be modified
Posted on July 03, 2003 at 13:05I've sorted the problem I had an unsed Port A (HS) configured as an input. Changing it to a output has solved the problem I'm still looking at ways of getting around the current used by the LVD on.
Posted on July 01, 2003 at 14:38St7lite2 I have a problem with ‘current’ on the ST7lite2 during the first 30 seconds after a reset. Too save ‘current’ I’m switching from slow to fast mode using an interrupt, which works OK. The problem is ...
Posted on February 11, 2003 at 12:29Re:Sorry I missed the dot! ... An external LVD sounds a good idea. Or could I connect a compactor from Ground to the reset pin to create a spike which will reset the processor. I’m using all the slow modes etc, ...