2007-05-06 10:18 PM
Programing Xflash while running from protected I-Flash
2007-05-06 8:47 PM
Hello all.
I was wonder whether can I program Xflash while running from protected I-Flash. Thanks. Ran2007-05-06 9:51 PM
Hello Ran,
It is possible to write the X-Flash while fetching from protected I-Flash. For more details, please refer to the ST10F276 datasheet, section 4.5.9 Access protection, Table 26, page 40/229. According to the table, when I-Flash is access protected, ''Read XFLASH/Jump to XFLASH and write Flash registers'' operations are allowed. Best regards, Najoua.2007-05-06 10:02 PM
Thanks.
Second Q: Can I run from Xflash and program It? (probably no, but what can lose?) Ran2007-05-06 10:18 PM
Hi again Ran,
The Flash 4 Banks (Bank0&1 in I-Flash and Banks 2&3 in X-Flash) have their own dedicated sense amplifiers, so that any Bank can be read while any other Bank is written. You can program Bank3 when fetching from Bank2 and conversely. During a Flash write operation, any attempt to read the bank under modification will output invalid data (software trap 009Bh). This means that the Flash Bank is not fetchable when a write operation is active. Best regards, Najoua.