2024-11-19 10:53 PM - last edited on 2024-11-20 08:01 AM by SofLit
A pattern is going to use P-NUCLEO-53L8A1 to monitor when a person get in to the bus , does anybody know how to send the information to the cloud via 4G or CAT and send GPS location, which devices should I use?
2024-11-21 08:19 AM
You are not about a specific problem of the P-NUCLEO-53L8A1, but about a complete solution for sending the data including the GPS location via 4G/CAT. In addition to the ToF sensor, you need at least two other devices:
You might consider the new low-power narrowband (NB-IoT) industrial module ST87M01 from STMicroelectronics, which also offers GNSS capability. The corresponding evaluation tool EVLST87M01 has already been announced and will hopefully be available soon.
Hope that helps?
Regards
/Peter
2024-11-25 10:31 AM
@Peter BENSCH wrote:You might consider the new low-power narrowband (NB-IoT) /Peter
@Jonamleonel mentioned this being on a bus - so, presumably, mobile ?
NB-IoT is not great for mobile applications!
LTE-M would be more suitable for a mobile application.
But these are both focussed on really power-constrained applications - which is probably not the case in a bus?
2024-11-25 10:37 AM - edited 2024-11-25 10:41 AM
The P-NUCLEO-53L8A1 is just a sensor evaluation kit:
https://www.st.com/en/ecosystems/p-nucleo-53l8a1.html
Sending data to the cloud really is an entirely separate issue - nothing to do with the sensors.
Data is just data - it makes no real difference where it came from.
There are dozens of different protocols that can be used to send data to the cloud:
https://www.google.com/search?q=microcontroller+send+data+to+cloud
If you want ST-specific material, try a search through the Knowledge Base; eg,