cancel
Showing results for 
Search instead for 
Did you mean: 

Hypertermial received strange data not as expected in baud rate 19200!

hg-chen
Associate II
Posted on May 25, 2007 at 12:37

Hypertermial received strange data not as expected in baud rate 19200!

4 REPLIES 4
hg-chen
Associate II
Posted on April 23, 2007 at 23:37

thank you,

It works in UART polling sample code!

in bps 9600 , the hyperterminal responds characters as I typed!

But when I configure as 19200, the hyperterminal responds data not as I typed, for example, I press ''Enter'' 4 times, the hyperterminal responds as 2 question mark ''? ?'' !?

anything wrong?

kaouther
Associate II
Posted on April 25, 2007 at 16:06

Could you please precise:

Which product? on which boards? which example used?

thanks.

hg-chen
Associate II
Posted on May 25, 2007 at 07:27

thank you for reply

basically the clock must be adjust to higher ! then the UART of PC receiving should be OK,

the STR711-SK/IAR tool set and the UART sample code is used ,

the RCCU sample code must also combined with UART sample code

to ensure it works also in high baud rates!

sofiene
Associate III
Posted on May 25, 2007 at 12:37

hi kuni,

Do you have always configuration problems with UART communication?

Regards,

M3allem