cancel
Showing results for 
Search instead for 
Did you mean: 

How can Flash running at 96MHZ

tiffanychen
Associate II
Posted on March 28, 2008 at 05:09

How can Flash running at 96MHZ

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
tiffanychen
Associate II
Posted on May 17, 2011 at 09:50

As title,

I use STR911FAM44X6, when I run flash up than 48MHZ the system hang...

So I only can run it on 48MHZ...

If some one knows solution, please kindly give me some advices...

Thank you very much

kais
Associate II
Posted on May 17, 2011 at 09:50

Dear tiffanychen,

Please verify the Flash wait states insertion when running above 48MHZ.

For example when running @96MHZ, Insert 2 Wait States for read:

FMI_Config(FMI_READ_WAIT_STATE_2, FMI_WRITE_WAIT_STATE_0, FMI_PWD_ENABLE,

FMI_LVD_ENABLE, FMI_FREQ_HIGH);

Kind regards,

Eris.

amira1
Associate II
Posted on May 17, 2011 at 09:50

Hello tiffanychen,

There is no problem with running flash above 48MHz. However, the maximum PCLK frequency is 48 MHz. Please find attached a simple example of toggling leds, flash running at 96MHz, and it's working well.

Please verify if you have something wrong in your software application.

Best regards,

Amira.

amira1
Associate II
Posted on May 17, 2011 at 09:50

Hello tiffanychen,

There is no problem with running flash above 48MHz. However, the maximum PCLK frequency is 48 MHz. Please find attached a simple example of toggling leds, flash running at 96MHz, and it's working well.

Please verify if you have something wrong in your software application.

Best regards,

Amira.

tiffanychen
Associate II
Posted on May 17, 2011 at 09:50

I'd already try the example from mirou,

but the system still hang...

Because the example is used for STR912...not STR911

so I just copy the clock setting part on my code

I also set the Wait state to 2, but it still can't run...

Please give me some advices if you have any idea...

Thank you very much

tiffanychen
Associate II
Posted on May 17, 2011 at 09:50

Can everybody help me?

Thank you very much