cancel
Showing results for 
Search instead for 
Did you mean: 

Help using SIMCom Y7080E on STM32L0

Andryck_Sant
Associate II

I would like to request assistance regarding an integration issue between my microcontroller(STM32L051C8T6) and the SIM Y7080E (an NB-IoT connectivity chip being used to publish messages via MQTT).

I am using an STM32L0 to control the SIM via UART, but for some reason, when I use the functions I wrote in a library to manage message transmission, the device responds that the message was successfully published to the MQTT broker. However, I cannot see the message using MQTT Explorer.

On the other hand, if I follow the same routine using commands by directly transmitting string content to the SIM via UART, the message gets published. Still, this doesn't always work either.

The difference is that in the first case, I concatenate strings and build the entire command body with the necessary information. In the second case, I assume the information is immutable and predefine it in the variable declaration for each command in the process.

I have reviewed all the documentation provided by the SIM manufacturer and followed the examples they supplied. With this approach, I successfully published messages by writing a test code in MicroPython (just to verify the device's functionality). However, the goal is to achieve the same result in C for this project. As mentioned earlier, on the STM32L0, I was only able to publish messages when the strings with the parameters were predefined. If I try to build the command in a transmission buffer, I receive a confirmation from the chip indicating the command is correct, but I notice that the MQTT broker does not receive any message.

Please, check the code below:

 

 

 

uint8_t y7080_mqtt_transmit(Y7080_HandleTypeDef *sim, uint16_t volume, float tension){

	uint8_t mqtt_topic[MQTT_TOPIC_SIZE], mqtt_payload[MQTT_PAYLOAD_SIZE], *aux;
	uint8_t mqtt_did[MQTT_DID_SIZE];


	memset(mqtt_did,0,MQTT_DID_SIZE);
	memset(mqtt_topic,0, sizeof(mqtt_topic));
	memset(mqtt_payload,0, sizeof(mqtt_payload));
	y7080_clear_buffer(sim);

	char mqtt_start_cmd[30],
	mqtt_accq_client[45],
	mqtt_topic_cmd[40],
	mqtt_payload_cmd[40],
	mqtt_pub_cmd[30],
	mqtt_disc_cmd[30];

	snprintf(mqtt_start_cmd, sizeof(mqtt_start_cmd),"%s",MQTT_START_CMD);
	snprintf(mqtt_accq_client, sizeof(mqtt_accq_client),"%s\"td_etc0\",0\r\n",MQTT_ACC_CLI_CMD);
	snprintf((char *)mqtt_topic, MQTT_TOPIC_SIZE, "marcosrangel/test\r\n");
	snprintf(mqtt_topic_cmd, sizeof(mqtt_topic_cmd), "%s%d\r\n",MQTT_WRITE_TOPIC_CMD,strlen((char *)mqtt_topic));
	snprintf((char *)mqtt_payload, MQTT_PAYLOAD_SIZE, "1234\r\n");
	snprintf(mqtt_payload_cmd, sizeof(mqtt_payload_cmd), "%s%d\r\n", MQTT_WRITE_PAYLOAD_CMD, strlen((char *)mqtt_payload));
	snprintf(mqtt_pub_cmd, sizeof(mqtt_pub_cmd), "%s1,60\r\n",MQTT_PUB_CMD);
	snprintf(mqtt_disc_cmd, sizeof(mqtt_disc_cmd), "%s",MQTT_DISCONNECT_CMD);

	HAL_UART_Transmit(sim->sim_uart, (uint8_t *)mqtt_start_cmd, strlen(mqtt_start_cmd),1000);
	y7080_wait_response(sim);
	y7080_clear_buffer(sim);

	HAL_UART_Transmit(sim->sim_uart, (uint8_t *)mqtt_accq_client, strlen(mqtt_accq_client),1000);
	y7080_wait_response(sim);
	y7080_clear_buffer(sim);


	aux = read_eeprom(8);
	memcpy(mqtt_did, aux, strlen((char *)aux));


	y7080_mqtt_connect(sim);
	y7080_clear_buffer(sim);


	HAL_UART_Transmit(sim->sim_uart, (uint8_t *)mqtt_topic_cmd, strlen(mqtt_topic_cmd),1000);
	y7080_wait_response(sim);
	y7080_clear_buffer(sim);

	if(HAL_UART_Transmit(sim->sim_uart, (uint8_t *)mqtt_topic, strlen((char *)mqtt_topic),1000) != HAL_OK){
		y7080_clear_buffer(sim);
		return 1;
	}
	y7080_wait_response(sim);
	y7080_clear_buffer(sim);



	if(HAL_UART_Transmit(sim->sim_uart, (uint8_t *)mqtt_payload_cmd, strlen(mqtt_payload_cmd), 1000)!= HAL_OK){
		return 1;
	}
	y7080_wait_response(sim);
	y7080_clear_buffer(sim);

	if (HAL_UART_Transmit(sim->sim_uart, mqtt_payload, strlen((char *)mqtt_payload), 1000) != HAL_OK){
		return 1;
	}
	y7080_wait_response(sim);
	y7080_clear_buffer(sim);



	if(HAL_UART_Transmit(sim->sim_uart, (uint8_t *)mqtt_pub_cmd, strlen(mqtt_pub_cmd), 1000)!= HAL_OK){
		return 1;
	}
	y7080_wait_response(sim);
	y7080_clear_buffer(sim);

	if(HAL_UART_Transmit(sim->sim_uart, (uint8_t *)mqtt_disc_cmd, strlen(mqtt_disc_cmd), 1000) != HAL_OK){
		return 1;
	}
	y7080_wait_response(sim);
	y7080_clear_buffer(sim);

	return 0;
}

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Andryck_Sant
Associate II

I found out the solution! The problem was the payload and the topic size.
If I want to send "1234" to the module as payload, I need to send the message with this structure:

"1234\r\n"

But I have to count only for bytes, because the last two indicates the end of the message. That's my mistake. I was sending payload size 6, while I was sending effectively 4 bytes. That, somehow was conflicting the module when it tried to pub the message.

 

Thanks for your help and attention.

View solution in original post

8 REPLIES 8

See here for tips on debugging serial comms:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/tac-p/706966/highlight/true#M49

 

BTW:

 


@Andryck_Sant wrote:

I am using an STM32L0 to control the SIM via UART


Your use of "SIM" here is confusing!

A "SIM" in the context of GSM Cellular Comms is the SIM card - one of these:

AndrewNeil_0-1736867190863.jpeg

(or the equivalent in chip form)

So you're not controlling the SIM - you're controlling the Y7080E module.

The module manufacturer is SIMCom.

Andryck_Sant
Associate II

Sorry about that! I got confused between module and SIM. In this case, my problem is specifically with the module.
I'm using STM32 Cube IDE version 1.17.0 to develop the mcu firmware.

 

I've already debugged the UART communication between the module and the mcu and everything seems to be ok. So, I can't understand why the message isn't appearing on the mqtt explorer.

I'll send attached bellow the image of the comm debug.

You said you have two cases - one works, and one doesn't.

So have you captured the comms traces in both cases, and compared them?

 

It would be clearer to post the trace as text rather than a screenshot - see here for preserving layout without adding syntax highlighting.

Not exactly, I had only captured the comm between the MCU and the Y7080E in C. After your sugestion that I have considered monitoring the comm between the MCU and Y7080E in uPython. I'll leave below both comms.

 

Note that UART0 = MCU and UART1 = Y7080E

Comm between MCU  and Y7080 in C:

UART0 -> UART1: b'AT\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CGDCONT=1,"IP","iot.datatem.com.br"\r\nAT+CGDCONT=1,"IP","i ot.datatem.com.br"\r\n'
UART1 -> UART0: b'\r\n+CME ERROR:8007\r\n\r\nOK\r\n'
UART0 -> UART1: b'AT+CGAUTH=1,1,"<apn_username>","<apn_psw>"\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CGATT=1\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CGDCONT=1,"IP","iot.datatem.com.br"\r\nAT+CGDCONT=1,"IP","i ot.datatem.com.br"\r\n'
UART1 -> UART0: b'\r\n+CME ERROR:8007\r\n\r\nOK\r\n'
UART0 -> UART1: b'AT+CGAUTH=1,1,"<apn_username>","<apn_psw>"\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CGATT=1\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTSTART\r\n'
UART1 -> UART0: b'\r\nOK\r\n\r\n+CMQTTSTART: 0\r\n'
UART0 -> UART1: b'AT+CMQTTACCQ=0,"td_etc0",0\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTCONNECT=0,"tcp://br1.data.fichar.io:1883",60,1,"<mqtt_broker_username>","<mqtt_broker_psw>"\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTTOPIC=0,19\r\n'
UART1 -> UART0: b'\r\n+CMQTTCONNECT: 0,0\r\n\r\n>\r\n'
UART0 -> UART1: b'marcosrangel/test\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTPAYLOAD=0,6\r\n'
UART1 -> UART0: b'\r\n>\r\n'
UART0 -> UART1: b'1234\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTPUB=0,1,60\r\n'
UART1 -> UART0: b'\r\nOK\r\n\r\n+CMQTTPUB: 0,0\r\n'
UART1 -> UART0: b'\r\n+CMQTTCONNLOST: 0,2\r\n'
UART0 -> UART1: b'AT+CMQTTTOPIC=0,19\r\n'
UART1 -> UART0: b'\r\n>\r\n'
UART0 -> UART1: b'marcosrangel/test\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTPAYLOAD=0,6\r\n'
UART1 -> UART0: b'\r\n>\r\n'
UART0 -> UART1: b'1234\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTPUB=0,1,60\r\n'
UART1 -> UART0: b'\r\nOK\r\n\r\n+CMQTTPUB: 0,26\r\n'

 


Check below the comm, between the MCU and the Y7080 in micropython.

UART0 -> UART1: b')\x89\x96\x80\xce\x11F\x11\x08\xbc1M)\x90i\x90\xa6!'
UART1 -> UART0: b'\r\n+POWERON:0\r\n\r\n^SIMST:1\r\n'
UART0 -> UART1: b'AT+NBAND=28\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CGDCONT=1,"IP","iot.datatem.com.br"\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CGAUTH=1,1,"apn_username","apn_psw"\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART1 -> UART0: b'\r\n+CEREG:2\r\n'
UART1 -> UART0: b'\r\n+CGEV:ME PDN ACT 1\r\n\r\n+CEREG:5\r\n'
UART0 -> UART1: b'AT\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+NCCID\r\n'
UART1 -> UART0: b'\r\n+NCCID:89550680157018171234\r\n\r\nOK\r\n'
UART0 -> UART1: b'AT+CPIN?\r\n'
UART1 -> UART0: b'\r\n+CPIN:READY\r\n\r\nOK\r\n'
UART0 -> UART1: b'AT+CSQ\r\n'
UART1 -> UART0: b'\r\n+CSQ:25,0\r\n\r\nOK\r\n'
UART0 -> UART1: b'AT+WORKLOCK=1\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CGATT=1\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CGATT?\r\n'
UART1 -> UART0: b'\r\n+CGATT:1\r\n\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTSTART\r\n'
UART1 -> UART0: b'\r\nOK\r\n\r\n+CMQTTSTART: 0\r\n'
UART0 -> UART1: b'AT+CMQTTDISC?\r\n'
UART1 -> UART0: b'\r\n+CMQTTDISC: 0,1\r\n\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTACCQ=0,"client_7830",0\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTCONNECT=0,"tcp://br1.data.fichar.io:1883",60,1,"broker_psw"\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART1 -> UART0: b'\r\n+CMQTTCONNECT: 0,0\r\n'
UART0 -> UART1: b'AT+CMQTTDISC?\r\n'
UART1 -> UART0: b'\r\n+CMQTTDISC: 0,0\r\n\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTSUB=0,23\r\n'
UART1 -> UART0: b'\r\n>\r\n'
UART0 -> UART1: b'marcosrangel2/teste/cfg\r\n'
UART1 -> UART0: b'\r\nOK\r\n\r\n+CMQTTSUB: 0,0\r\n'
UART0 -> UART1: b'AT+CMQTTTOPIC=0,19\r\n'
UART1 -> UART0: b'\r\n>\r\n'
UART0 -> UART1: b'marcosrangel2/teste\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTPAYLOAD=0,612\r\n'
UART1 -> UART0: b'\r\n>\r\n'
UART0 -> UART1: b'{"timestamp": 1730490841, "unique_id": "e05a1b196b84", "dev_info": {": 117672, "bat_voltage": 7.2, "flag": "18", "pw_status": "CONNECTED", "cpu_temp": 55._usage": 60.5, "ip": "192.168.0.218", "pw_voltage": 7.2, "timezone": 0, "firmware_vers
UART0 -> UART1: b'n": "1.19.1"}, "payload": {"b170 - GC": {"max": 10100, "val": 4206.1g": 0, "min": 0, "unt": "L"}, "b185 - GA": {"max": 10100, "val": 6625.325, "trg": 0, ", "unt": "L"}, "B177 - ET": {"max": 15600, "val": 4618.672, "trg": 0, "min": 0, "unt":
UART0 -> UART1: b'L"}, "b171 - S10": {"max": 10100, "val": 0, "trg": 0, "min": 0, "unt}, "format": "fichario"} \r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CMQTTPUB=0,1,60\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART1 -> UART0: b'\r\n+CMQTTPUB: 0,0\r\n'

 

 

So have you done a side-by-side comparison of the two?

They seem quite considerably different.

eg, your CGDCONT gives an error in the C case:

UART0 -> UART1: b'AT\r\n'
UART1 -> UART0: b'\r\nOK\r\n'
UART0 -> UART1: b'AT+CGDCONT=1,"IP","iot.datatem.com.br"\r\nAT+CGDCONT=1,"IP","i ot.datatem.com.br"\r\n'
UART1 -> UART0: b'\r\n+CME ERROR:8007\r\n\r\nOK\r\n'

 

And your CMQTTCONNECT commands differ

UART0 -> UART1: b'AT+CMQTTCONNECT=0,"tcp://br1.data.fichar.io:1883",60,1,"<mqtt_broker_username>","<mqtt_broker_psw>"\r\n'
UART0 -> UART1: b'AT+CMQTTCONNECT=0,"tcp://br1.data.fichar.io:1883",60,1,"broker_psw"\r\n'

 

 

BTW: How to post "formatted" text without syntax highlighting:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/tac-p/725146/highlight/true#M54

Andryck_Sant
Associate II

I found out the solution! The problem was the payload and the topic size.
If I want to send "1234" to the module as payload, I need to send the message with this structure:

"1234\r\n"

But I have to count only for bytes, because the last two indicates the end of the message. That's my mistake. I was sending payload size 6, while I was sending effectively 4 bytes. That, somehow was conflicting the module when it tried to pub the message.

 

Thanks for your help and attention.


@Andryck_Sant wrote:

I found out the solution! .


Excellent - so please mark your post as the solution:

https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

 


@Andryck_Sant wrote:

I need to send the message with this structure:

"1234\r\n"

But I have to count only for bytes, because the last two indicates the end of the message. That's my mistake. I was sending payload size 6, while I was sending effectively 4 bytes. .


I don't follow: "1234\r\n" is 6 bytes:  four digits, then a CR, then a LF - a total of 6.

Andryck_Sant
Associate II

It can be a little confusing. lol
The last two bytes must be the message terminators. So the Y7080E can recognize the end of the message(you have to follow this pattern to all commands). In the case that you need to break a line on the payload you should send:

"1234\r\n\r\n"

6 bytes are for the message payload and the last 2 are for the Y7080E recognize the end of the payload or command. But you have a total of 8 bytes sent. 6 for payload and 2 for the Y7080E.