2004-04-01 11:35 AM
Evaluation board, can anyone help me, please ??
2011-05-17 2:59 AM
I´m working with the evaluation board M41ST87 of ST, and I want to text the line P1_0 of the uProcesador, this line is the CPU_ADC0, pin 52, if I want to output in this line one alternaty line, I have programmed the next, and is impossible to see with the osciloscoper the right signel, I don´t kown why ?
P1SFS0 = 0x00; // port 1 of uP, like GPIO P1_0 = ~P1_0; // change the line constinuosly In the windows of the pararell port, appears the signal P1_0 changing, but with the osciloscoper in pin 52 is impossible to see it, Why ?2011-05-17 2:59 AM
I assume you are using a DK3300 board since the M41ST87 is a Real Time Clock chip (and is on the DK3300 board).
I suspect that you did not define port 1.0 pin function as ''GP I/O mode'' in PSDsoft when you were configuring the device. Go back to PSDsoft and define that pin as such.