cancel
Showing results for 
Search instead for 
Did you mean: 

problem in programming through JTAG

babidesai123
Associate II
Posted on March 30, 2004 at 17:39

problem in programming through JTAG

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
babidesai123
Associate II
Posted on May 17, 2011 at 11:59

hello,

I am using the uPSD323X from last one year. But for the first time i could see that the chip already programmed through JTAG ( more that 5 times)is not getting reprogram/erase.

It's not able to communicate through JTAG . but the previous loaded image is working fine

IT SHOWS: MISMATCH OF IDCODE

here is the attached log file generated

PLZ help

Purvi
babidesai123
Associate II
Posted on May 17, 2011 at 11:59

hello,

i have not changed the user code from the default FFFFFFFF value.

regards

purvi
jdaniel
Associate II
Posted on May 17, 2011 at 11:59

Purvi,

I've seen this message if I accidentally have the wrong uPSD product selected in the JTAG programming screen within PSDExpress. For instance, if I was trying to program a uPSD3254A and I had selected the PSD854 as the device in the JTAG operation dialog box, it will show this error. Maybe take a look at this dialog (or your .jcf file if you're using it from the command line) and make sure it matches.

Best Regards,

Phaze426