2008-12-24 2:02 AM
2011-05-17 12:57 AM
I need to address the ext. memory (21e00000) in ST91x. I have configured the EMI as follow but still failed~ can you help me?
GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 |GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt3; GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Disable; GPIO_Init (GPIO5, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2; GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Disable; GPIO_Init (GPIO7, &GPIO_InitStructure); GPIO_Init (GPIO8, &GPIO_InitStructure); GPIO_Init (GPIO9, &GPIO_InitStructure); // those bastards. this one pin out of 24 is on a different alt bus GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt3; GPIO_Init (GPIO7, &GPIO_InitStructure); // configure SCU SCU_EMIModeConfig(SCU_EMI_DEMUX); SCU_EMIBCLKDivisorConfig(SCU_EMIBCLK_Div1); // or SCU_EMIBCLK_Div1; SCU->GPIOEMI = 1; // enable ports 8 & 9 for EMI GPIO_EMIConfig( ENABLE ); /* Enable EMI clock */ EMI_DeInit(); EMI_StructInit( &eMI_InitStruct ); eMI_InitStruct.EMI_Bank_MemWidth = EMI_Width_HalfWord; eMI_InitStruct.EMI_Bank_IDCY =0x6; eMI_InitStruct.EMI_Bank_WSTRD =0x6; eMI_InitStruct.EMI_Bank_WSTWR =0x6; eMI_InitStruct.EMI_Bank_WSTROEN=0x6; eMI_InitStruct.EMI_Bank_WSTWEN=0x08; eMI_InitStruct.EMI_Bank_MemWidth=EMI_Width_HalfWord; EMI_Init( EMI_Bank1, &eMI_InitStruct );2011-05-17 12:57 AM
Hi
As I can see in your peace of code the configuration of GPIO8&9 is wrong. Please refer to the STR9 EMI application note available on the web: It contains several software examples configuring the EMI in several modes. Kind regards, Eris2011-05-17 12:57 AM
Thx.. Can you give me the sample? I changed to:
SCU_APBPeriphClockConfig(__GPIO0, ENABLE); SCU_APBPeriphClockConfig(__GPIO4, ENABLE); SCU_APBPeriphClockConfig(__GPIO5, ENABLE); SCU_APBPeriphClockConfig(__GPIO7, ENABLE); SCU_APBPeriphClockConfig(__GPIO8, ENABLE); SCU_APBPeriphClockConfig(__GPIO9, ENABLE); //led GPIO_DeInit(GPIO4); GPIO_StructInit(&GPIO_InitStruct); GPIO_InitStruct.GPIO_Direction = GPIO_PinOutput; GPIO_InitStruct.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_7; GPIO_InitStruct.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStruct.GPIO_Alternate = GPIO_OutputAlt1; GPIO_Init(GPIO4, &GPIO_InitStruct); //P5.0, 5.1 GPIO_DeInit(GPIO5); GPIO_StructInit(&GPIO_InitStruct); GPIO_InitStruct.GPIO_Direction = GPIO_PinOutput; GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1; GPIO_InitStruct.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStruct.GPIO_Alternate = GPIO_OutputAlt1; GPIO_Init(GPIO5, &GPIO_InitStruct); GPIO_WriteBit(GPIO5, GPIO_Pin_0, 0); GPIO_WriteBit(GPIO5, GPIO_Pin_1, 1); //EMI , P0.4:cs0 P0.5:cs1 GPIO_DeInit(GPIO0); GPIO_StructInit(&GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 |GPIO_Pin_6|GPIO_Pin_7; GPIO_InitStruct.GPIO_Direction = GPIO_PinOutput; GPIO_InitStruct.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStruct.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init(GPIO0, &GPIO_InitStruct); //P7.0-P7.6:A16-A22; P8.0-P9.7:AD0-AD15 GPIO_DeInit(GPIO7); GPIO_StructInit(&GPIO_InitStruct); GPIO_InitStruct.GPIO_Direction = GPIO_PinOutput; GPIO_InitStruct.GPIO_Pin = GPIO_Pin_All; GPIO_InitStruct.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStruct.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init(GPIO7, &GPIO_InitStruct); GPIO_DeInit(GPIO8); GPIO_StructInit(&GPIO_InitStruct); GPIO_InitStruct.GPIO_Direction = GPIO_PinOutput; GPIO_InitStruct.GPIO_Pin = GPIO_Pin_All; GPIO_InitStruct.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStruct.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init(GPIO8, &GPIO_InitStruct); GPIO_DeInit(GPIO9); GPIO_StructInit(&GPIO_InitStruct); GPIO_InitStruct.GPIO_Direction = GPIO_PinOutput; GPIO_InitStruct.GPIO_Pin = GPIO_Pin_All; GPIO_InitStruct.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStruct.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init(GPIO9, &GPIO_InitStruct); //P7.7:A23 GPIO_InitStruct.GPIO_Pin = GPIO_Pin_7; GPIO_InitStruct.GPIO_Alternate = GPIO_OutputAlt3; GPIO_Init(GPIO7, &GPIO_InitStruct); SCU_EMIModeConfig(SCU_EMI_MUX); SCU_EMIALEConfig(SCU_EMIALE_LEN2, SCU_EMIALE_POLHigh); SCU_EMIBCLKDivisorConfig(SCU_EMIBCLK_Div2); GPIO_EMIConfig(DISABLE); SCU_AHBPeriphClockConfig(__EMI, ENABLE); EMI_DeInit(); EMI_StructInit(&EMI_InitStruct); EMI_InitStruct.EMI_Bank_MemWidth = EMI_Width_HalfWord; EMI_InitStruct.EMI_Bank_IDCY = 0x3;// bus turnaround cycle EMI_InitStruct.EMI_Bank_WSTROEN = 0x06; //output enable assertion delay EMI_InitStruct.EMI_Bank_WSTRD = 0x06;// read wait state EMI_InitStruct.EMI_Bank_WSTWEN = 0x08;// write enable assertion delay EMI_InitStruct.EMI_Bank_WSTWR = 0x06;// write wait state EMI_InitStruct.EMI_Bank_MemWidth = EMI_Width_HalfWord; EMI_Init(EMI_Bank0, &EMI_InitStruct); EMI_Init(EMI_Bank1, &EMI_InitStruct); EMI_Init(EMI_Bank2, &EMI_InitStruct); EMI_Init(EMI_Bank3, &EMI_InitStruct);2011-05-17 12:57 AM
Do you enable EMI_MEM_CLK?
SCU_AHBPeriphClockConfig(__EMI_MEM_CLK, ENABLE);2011-05-17 12:57 AM
Hi,
As I can understand from your peace of code you want to configure STR9 EMI in Mux mode. Well, the software of Mux_Mode_SRAM example accompanied with the AN2647 Can be a good demonstration for you (Please find it attached). You have only to modify the chip select GPIO configuration since you are using GPIO0 pins as chip select instead of GPIO5. You have also to use the appropriate wait states related to the connected memory otherwise the Read or write access operations can not be performed. Kind regards, Eris.