2005-07-18 8:42 PM
2005-07-18 8:42 PM
I have found some inconsistences between the datasheet and the 71x_lib to do with the APB regisiters.
In version 6 of the STR71x data sheet(p338) it clearly states ''Bit 0 controls the peripheral in position 1 (I2C0 for APB1 or XTI for APB2) and so on''. However if you look at the #define in APB.h these are wrong and start at bit 1 from apb.h v3.0 (latest version on st web site) /* APB1 Peripherals */ #define I2C0_Periph 0x0002 #define I2C1_Periph 0x0004 #define UART0_Periph 0x0010 #define UART1_Periph 0x0020 #define UART2_Periph 0x0040 #define UART3_Periph 0x0080 #define USB_Periph 0x0100 #define CAN_Periph 0x0200 #define BSPI0_Periph 0x0400 #define BSPI1_Periph 0x0800 #define HDLC_Periph 0x2000 /* APB2 Peripherals */ #define XTI_Periph 0x0002 #define GPIO0_Periph 0x0004 #define GPIO1_Periph 0x0008 #define GPIO2_Periph 0x0010 #define ADC12_Periph 0x0080 #define TIM0_Periph 0x0200 #define TIM1_Periph 0x0400 #define TIM2_Periph 0x0800 #define TIM3_Periph 0x1000 #define RTC_Periph 0x2000 #define WDG_Periph 0x4000 #define EIC_Periph 0x8000 Also the EIC_Periph is placed at bit 15 even though the datasheet would appear to have bit 15 as a reserved bit. Although the discription is not clear as the text doesnt mention bit 15. from datasheet - Bit 31:16 = Reserved, must be kept at reset value (0). Bit 14:0 = Peripheral Clock Disable (14:0) What happend to bit 15 ? Perhaps on the next release of the 71x library/datahseet you could correct whichever is wrong. Ben