2024-12-14 1:18 AM
hi,
I need to make a database storage ( 20GB ) place using FatFs So, stored data's will be retained from the storage place and stored data's will come to display when necessary .
1. Full Speed USB Flash Drive as Storage - Decent Speed but most of the USB Flash Drive are getting Hot for long time in PC . I didn't tested hotness of USB Flash Drive plugged with stm32 for 24 hours . it's really worth consider the USB Flash Drive as Storage based on the failure circumstance .in case if i choose the USB HDD based SSD or NVMe as Storage then Size too big and cost . There is any rugged USB Flash Drive ?.
2. SD Card as Storage - SD card life is unpredictable .
3. eMMC as Storage (i don't have Experience using eMMC) - will stm32 mcu support in eMMC 4 bit mode as sd card using FatFs ? and Not interest for 8 bit mode eMMC since many works involved for using FatFs or little FatFs.
who will be runner up for speed and life of storage device ? with following combination.
stm32 + USB Flash Drive ( Pendrive ) .
stm32 + USB HDD based on SSD or NVMe as Storage .
stm32 + eMMC ( 4bit Mode SD Card Mode ) .
Please share your technical tips and suggestion .
2024-12-14 3:28 AM
@MMARI.1 wrote:most of the USB Flash Drive are getting Hot for long time in PC
Are you sure that's due to the drive itself? Could well be heating from the PC ...
@MMARI.1 wrote:SD card life is unpredictable .
Is it? I don't think that SD-Cards are inherently any more nor less "reliable" than comparable USB sticks?
@MMARI.1 wrote:There is any rugged USB Flash Drive ?.
What, exactly, do you mean by "rugged" ?
maybe try
https://nexusindustrialmemory.com/
https://shop.sandisk.com/products/memory-cards/microsd-cards/industrial-microsd?sku=SDSDQAF3-008G-I
https://shop.sandisk.com/products/embedded-flash/industrial-inand-emmc-drives?sku=SDINBDG4-8G-I2
2024-12-22 1:56 AM - last edited on 2024-12-23 1:15 AM by Andrew Neil
Hi Neil,
Do you think using Portable HDD ( SSD based) + USB high speed driver + stm32 mcu will give the best data transfer rate? .
2024-12-22 3:04 PM
FATFS will work with whatever you implement in the DISKIO layer
I'd use current version of FATFS, not the one from 2017. Efficiency/speed will come from using large aligned blocks, spanning multiple sectors, ideally cluster sizes, or 32KB, or whatever you can accomodate. Doing many small transactions at an application level will kill speed.
2024-12-22 7:26 PM - edited 2024-12-23 12:49 AM
hi,
Database look like this .
single folder maximum size will be 3MB (mega byte) and most of the time folder size will be less than 3MB. Day wise folder will be called one by one to Display Buffer.
Still i am not come to the conclusion to use USB based HDD or SDMMC based eMMC !.
Theoretically going through to both memory device with following consideration .
1. Long Life 2. Stability ( No frequent crash ) 3. Speed .
FatFs SFN vs FatFs LFN will make impact on Speed ?.
How much industrial SDMMC card is good in 1. Long Life 2. Stability ( No frequent crash ) 3. Speed compared to micro SD card . Since this Card has been used in Camera .
For eMMC below link case study will be useful .
FatFs 32bit vs FatFs 64 bit
if you have any technical suggestion (or) tips are most welcome on this subject .