2024-12-14 01:18 AM
hi,
I need to make a database storage ( 20GB ) place using FatFs So, stored data's will be retained from the storage place and stored data's will come to display when necessary .
1. Full Speed USB Flash Drive as Storage - Decent Speed but most of the USB Flash Drive are getting Hot for long time in PC . I didn't tested hotness of USB Flash Drive plugged with stm32 for 24 hours . it's really worth consider the USB Flash Drive as Storage based on the failure circumstance .in case if i choose the USB HDD based SSD or NVMe as Storage then Size too big and cost . There is any rugged USB Flash Drive ?.
2. SD Card as Storage - SD card life is unpredictable .
3. eMMC as Storage (i don't have Experience using eMMC) - will stm32 mcu support in eMMC 4 bit mode as sd card using FatFs ? and Not interest for 8 bit mode eMMC since many works involved for using FatFs or little FatFs.
who will be runner up for speed and life of storage device ? with following combination.
stm32 + USB Flash Drive ( Pendrive ) .
stm32 + USB HDD based on SSD or NVMe as Storage .
stm32 + eMMC ( 4bit Mode SD Card Mode ) .
Please share your technical tips and suggestion .
2024-12-14 03:28 AM
@MMARI.1 wrote:most of the USB Flash Drive are getting Hot for long time in PC
Are you sure that's due to the drive itself? Could well be heating from the PC ...
@MMARI.1 wrote:SD card life is unpredictable .
Is it? I don't think that SD-Cards are inherently any more nor less "reliable" than comparable USB sticks?
@MMARI.1 wrote:There is any rugged USB Flash Drive ?.
What, exactly, do you mean by "rugged" ?
maybe try
https://nexusindustrialmemory.com/
https://shop.sandisk.com/products/memory-cards/microsd-cards/industrial-microsd?sku=SDSDQAF3-008G-I
https://shop.sandisk.com/products/embedded-flash/industrial-inand-emmc-drives?sku=SDINBDG4-8G-I2