2004-07-04 1:13 AM
compiler C to OBJ & HEX (for DK3200)
2011-05-17 3:02 AM
Hello !
i am a newbie in this bussiness and I need your immediate help . Where can I get a compiler from C to OBJ and HEX? Thanks for your attention . jeniok2011-05-17 3:02 AM
Hi
I guess you can ask the dealer from where you got the DK3200 to give you an evaluation copy of the C compiler, which would give you both the obj and hex files. You can use Keil C compiler for the same. I dont rember if you get is along with the DK3200 kit. Check it out Wish you good luck and prosperity in your business!2011-05-17 3:02 AM
Can you send me the exact link where I can download the compliler?
There are many compilers and I don't find where to download the one I need, I don't know which one I need to compile from C to OBJ and HEX.2011-05-17 3:02 AM
There are numerous compilers available for the upsd, any which support 8032 core.
Have a look at www.keil.com, www.raisonance.com, www.tasking.com etc. If you want to go the free route have a look at sdcc Regards sjo2011-05-17 3:02 AM
Yes sjo is right.
For DK3200 using UPSD3200, you need to have Keil C compiler. With this, you can compile may devices, e.g Philips 5051 core family , Philips 8032 famliy processors or Cygnal processors etc. So you are not restricted with only 1 type of devices. You get a demo CD from them which has got demo programs and tutorials for using the Keil compiler. Have fun !