cancel
Showing results for 
Search instead for 
Did you mean: 

Can Port1.11 act as external interrupt

jjmicro
Associate II
Posted on March 31, 2006 at 12:29

Can Port1.11 act as external interrupt

4 REPLIES 4
jjmicro
Associate II
Posted on March 31, 2006 at 06:54

Port1.11 set as INPUT port ,Can it raise an external interrupt

triggering on the rising edge ?

hichem2
Associate II
Posted on March 31, 2006 at 07:20

Hi,

All the The IRQ & FIQ Interrupt vector are illustrated in table 23 & 24 (page 81/349) of the STR71x Ref Man Rev .7

regards,

Hich

jjmicro
Associate II
Posted on March 31, 2006 at 09:04

Pls tell me whether Port1.11 can raise an interrupt when it setting as INPUT port and CONTROLLER AREA NETWORK is disable !

hichem2
Associate II
Posted on March 31, 2006 at 12:29

Hi jjmi,

As Table 26 page 103/349, P1.11 can be configured as an External Interrupt Line source.

regards,

Hich