cancel
Showing results for 
Search instead for 
Did you mean: 

Why I'm not getting the list of targets inside Flash Loader Demonstrator(Version-2.8),

Axay
Associate II

I'm using the STM32 H7A3Zi-Q Nucleo-144 development kit. While I'm trying to enter to the bootloader by connecting BOOT0 pin to the 3V3(VDD) pin & I'm using the ST toll called Flash Loader Demonstrator in order to achieve the same. While I'm doing it so, I'm not getting the list for the target

0693W00000UnutAQAR.png0693W00000UnutKQAR.png

1 ACCEPTED SOLUTION

Accepted Solutions

This is an old tool not supporting the H7 and not being maintained.

Use STM32 Cube Programmer as it also supports USB and UART based connectivity to the ROMs system loader.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

1 REPLY 1

This is an old tool not supporting the H7 and not being maintained.

Use STM32 Cube Programmer as it also supports USB and UART based connectivity to the ROMs system loader.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..