cancel
Showing results for 
Search instead for 
Did you mean: 

How to add constant voltage and constant current circuit in VIPER35 based SMPS design

Zope
Associate

Hello, I want to design the SMPS (Isolated fly back with opto coupler) have output of 10V and 1.5A (i.e 15W) with constant voltage (CV) and constant  current (CC) with input range 90V to 265V, 50Hz, i selected VIPER35HD chip for this design with eDesignSuite, but not able to added the CV/CC in the design input specification, because we need CC to charge the Li-Ion battery. Can someone help, how i can add the CV/CC in edesignsuite.

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @Zope, to the community!

A primary controlled flyback power supply requires help from a special CC/CV controller such as the SEA05 or SEA05L to map the two control information CC and CV to the feedback channel. There are also technical notes and application notes on their product websites that show their application using an example.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks, will check.