cancel
Showing results for 
Search instead for 
Did you mean: 

Wierd problem

vividmusic
Associate II
Posted on February 11, 2005 at 04:33

Wierd problem

2 REPLIES 2
vividmusic
Associate II
Posted on February 08, 2005 at 21:21

Hi there

I recently migrated from 98 to XP and now there is one pin on port E that i cant use. Im using 5 Ive deleted every thing except the code to toggle PE3 but still no toggleing. Can anyone see anything that im missing? Has this happened to anyone?Ive tried it on different 521 and on Im using cosmic compiler and indart ST7F programmer

Thanks for your help

Chris

________________

Attachments :

TEST.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzup&d=%2Fa%2F0X0000000bTX%2FocoplFKIeQBOMuilp09D7QScBOKX23EHR2jpSJ0CMkg&asPdf=false
luca239955_st
Associate III
Posted on February 11, 2005 at 04:33

Chris,

from the compiler point of view I'm confident there is no difference between different versions of windows (provided that you are using the same compiler version everywhere, of course).

Anyway, that's easy to check; just compare the hex files on the 2 systems and see if they are the same.

Regards,

Luca (Cosmic)