2007-11-21 03:46 AM
2006-11-13 09:15 AM
Hi all,
seems like I deleted bootloader sector from system memory.Is it possible to get file for programming this flash zone ?2006-11-14 03:07 AM
2006-11-14 04:31 AM
Quote:
On 14-11-2006 at 16:37, Anonymous wrote: Hello, The STR75x bootloader can not be deleted nor programmed by User or by any programming tool in the Market. This can be done only in STMicroelectronics. For sure, you have something wrong in your configuration, Could you please check your Boot mode and if you are booting from the right SystemMemory Mode. For more details you can refer to ''AN2430 : STR75x SystemMemory boot mode'' With best regards, Rave Hi, it is very strange... I set BOOT0 = 1 (Vcc) , BOOT1 = 0 (GND) , GPIO0.4 = 0 (Gnd) and after RESET I send 0x7F to comport0 . I have to get back 0x75 but don't get any characters.I am using Keil demo board.2006-11-15 10:13 PM
Hello,
That's stange! What is the date code of the STR752 chip on Keil board? just send us all infos written on STR752 package. Thanks.2006-11-15 11:19 PM
Quote:
On 16-11-2006 at 11:43, Anonymous wrote: Hello, That's stange! What is the date code of the STR752 chip on Keil board? just send us all infos written on STR752 package. Thanks. MCBSTR750 Vers.1 MCU: STR750FV2T6 Z 22 024 V6 MLT 22 6302006-11-22 10:59 AM
I'm having this same identical problem on an IAR STR750-SK rev B evaluation board, although I encountered it with a virgin board (no chance of accidentally erasing anything.)
My STR750 Chip says: STR750FV2T6 Z 22 024 VG MLT 22 630 Which is identical to the previous posters, except I think they may have misread a ''G'' as a ''6''...2006-11-22 09:03 PM
Quote:
On 23-11-2006 at 00:29, Anonymous wrote: I'm having this same identical problem on an IAR STR750-SK rev B evaluation board, although I encountered it with a virgin board (no chance of accidentally erasing anything.) My STR750 Chip says: STR750FV2T6 Z 22 024 VG MLT 22 630 Which is identical to the previous posters, except I think they may have misread a ''G'' as a ''6''... Hi, I got a message from ST that this revision don't has properly working bootloader :-[2006-11-23 06:33 AM
Hi all,
Yes, all the starter kits from IAR,Keil, Hitex, Raisonnance and ST already you are using have an early version of silicon that does not contain the bootloader as described in the Application Note. You have to contact ST Sales to get the new samples shipped from the begining of September when the STR750 product is launched and try to rework the chip in your board. With best regards :-)2006-12-04 07:56 PM
Hi All,
Please find the answer to these questions in the A.N2430 ''STR75x SystemMemory boot mode''. There is a detailed section for the bootloader availability on the devices. I attached the A.N , also available on the web site. With Best Regards, ________________ Attachments : AN2430.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtRS&d=%2Fa%2F0X0000000aQ5%2F04zP0A3dXtgZoJYnlLAUtgtstQw.UmeQtykFEIFa1Lg&asPdf=false