2003-11-21 12:41 AM
STPC Vega : Finding a tri-state output
2003-11-17 12:34 AM
Do you know the default state of GPIO (before initialization).
I need an ouput in tri-state before bios has finish is initialization. thanks. [EMAIL]null[/EMAIL][EMAIL]null[/EMAIL]2003-11-21 12:41 AM
After reset, GPIOs are in input. This means that SPTC is not driving it. Depending on what you have on boards, if no-one else is driving it, then it will be in tri-state.
They remain in this condition until they are initialised, that is when the system needs them.