2003-07-23 03:43 AM
2003-05-18 10:53 PM
Hello All ,
I want to use the ST7Lite05 with the Internal RC oscillator and to work with the SCI (RS232) communication . Do you think that there will be a problem with the communication in several computers because of the accuracy or not ? Shermantec2003-05-19 02:54 AM
Internal RC has an accuracy of 1% as specified into the datsheet.
2003-07-22 04:31 AM
With RC clock You will have bit sample problems during a receiver session, with higher baud rates. I have used this solution with satisfaction for baud rates lower than 2000 bps.
2003-07-22 11:55 PM
Hi,
I'm running at 9600 with no problem. The only risk is when the supply changes,as this will change the clock freq. Simon Anglia2003-07-23 03:43 AM
I have tested it from 2.4kbps to 19.2kbps without any problem with internal RC clock.