cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 custom board hardware errors

BKN636
Associate II

Hello everyone,

im currently working on a custom pcb which uses the STM32L031K6 and im having some troubles with it.

Ive attatched the schematic and some oscilloscope measurements.

Fault description:

-random signals and floating voltage levels on various I/O pins

-fault occurence ranges from minutes to hours

-3rd board revision, changed several periphal ICs, same error pattern

-errors seems to occur at random, even when the board is in idle (no h bridge switching)

Board I/O:

-rs232 via uart (MAX3250)

-12bit dac via i2c (MCP4725)

-16bit adc via spi (INA240+ ADS8864)

-3 digouts for h bridge control (no pwm, just steady state enable/disable)

-1 digout for current control ic (drv110), gives static enable signal (drv110 drives h-bridge low side switch via pwm)

-2 digouts for led

-1 internal 12bit adc

Supply:

-24V lab supply behind transformer

Debug probe:

-Segger J link edu mini via usb isolator

Things ive tried:

-closely observed 3v3 supply, seems clean, no overvoltage during start up or sudden shut downs, tried several different switching controllers on each board revision, all seemed fine to me

-tried several compilers, eclipse, keil & atollic, projection creation & µC initialisation via cubemx, created projects with "normal code" (which seems to run decent on some board revisions), and some with no functional code with setting all digouts to zero

-tried all combinations for digouts & alternate functions, pushpull, open drain, /w & w/o pullup/pulldowns

-replaced µC numerous times, all seem to get faulty after a while (perhaps faulty batch/damage during storage?)

-obviously the i/o ports seemed to get damaged, but why several at the same time?

Appreciate any help from you guys.

Kind regards

This discussion is locked. Please start a new topic to ask your question.
21 REPLIES 21
TDK
Guru

Once it occurs, it doesn't recover, right? Which pins in particular get damaged? Always the same ones?

Sounds like a hardware issue, probably overvoltage on pins due to some external source, maybe during inrush or some other event. Use the information about which pins are damaged to track down the issue. Are pins ever powered while the chip is off (VDD=0)?

If you feel a post has answered your question, please click "Accept as Solution".
andy2399
Senior

You don't seem to have the RESET pin pulled high.

A floating reset pin may give you periodic problems.

Andy

Tilen MAJERLE
ST Employee

The STM32L0 has an internal pullup on NRST.

If you feel a post has answered your question, please click "Accept as Solution".
JGerb
Associate III

My 2c worth (forgive me if I explain what may be obvious):

It looks like your boards have isolation, perhaps motor controllers, and some high current / high-voltage stuff going on. I'd have a look to make sure something in this environment isn't killing your micro :

1) That micro has no clamps for positive over-voltage on the I/O. Thus it can be broken easily by any kind of inductive spikes or ground bounce. When a pin dies, try measuring resistance to ground and to +3V3. That may give you some clues. Also check the resistance values while the micro is powered up and while off. If you see a resistance path to GND in the order of kΩ, suspect a HV spike with low energy behind it. If you see ohms, something with current behind it has trashed the pin. See if you can still measure the negative clamping diode for the pin to check if it's still there. If you have inputs coming from off-board or high-current/voltage sources, isolate with a few hundred to a few kiloohms in series (Adjust R53 according to your needs), AND add a clamp to supply, and then another resistor in series as well (R3 can be as low as 100 ohms, but do your calculations assuming an ESD hit of 8kV from a 2k source) - if there is e.g. a negative going spike, you don't want the current shared between your protection diode and the internal protection diode. I use the scheme below for all inputs that travel any distance or to a pushbutton or LED anything that might pick up static from a user/machine. A BAV99 can take 2 or 4A for a microsecond and is almost free and has practically no leakage. If you can't clamp to your 3V3 rail due to too little current draw (micropower designs e.g.) then clamp to a shared transzorb, even if you have to pre-bias it to supply.

0693W000001pPMrQAM.png

2) Check your grounds. Make sure there is no ground shift happening due to high currents in the groundplane/fill. Make sure both VSS pins are connected to each other very solidly, and to same GND as your input signals. If you have high current, make sure your micro is on its own, quiet, ground with no current flowing in it. And a nice ground fill underneath it if you can. If you're on a 2-layer PCB, you may struggle. Check for placement of switching regulators and other sources close to the micro, especially keep the SW pin away from the micro.

3) The input pins can't be damaged by a 3.3V signal injected when the micro is off, you'd have to go > 4V above Vdd to do that. But it can be damaged by negative going signals in excess of 20mA.

4) Suspect the firmware. If you can reproduce the fault, try and get debug output of the GPIO registers of the affected ports.

5) Check for EMC. If you don't have equipment for this, take a seek coil out of an old hard drive and wire to a BNC into your oscilloscope. Wave it around in the vicinity of the PCB and play "warmer warmer colder colder" till you can see what's coming out of where.

6) Check that reset line - I think there's supposed to be a 1k resistor in series with the cap on the reset line. And a push-button can be a nice place for static to enter a micro, so consider whether it needs a clamp.

7) Check the layout carefully, look for routing of all pins going to the micro. If they run close to high dv/dt nodes, especially for long runs, you need to shift them elsewhere.

Dvorak.Peter
Senior II

It looks to me that this schematic is haunted by evil spirits from the past.

The so called bridge driver is :

FDMQ8205A is GreenBridgeTM2 series of quad MOSFETs for a bridge application so that the input will be insensitive to the polarity of a power source 

BKN636
Associate II

Thank you for your input so far guys. Ill much appreciate any new ideas. Especially after a few weeks of being stuck...

Ive uploaded the PCB and a measurement of the Vdd supply.0693W000001pQWiQAM.bmp

BKN636
Associate II

It seems to me that most of the I/O Pins get faulty from time to time. That includes UART, I2C and Digouts. However they dont seem to recover after the board has been powered off for a while.

BKN636
Associate II

0693W000001pQqnQAE.pngReset connection looks to be in order when checking the HW guideline.