Posted on May 17, 2011 at 11:55Hi, The idea of I2C is to allow numerous devices to communicate over only two wires. no other chip selects are requried. When you look in the datasheet for the devices you are going to use, you will see that each devic...
Posted on May 17, 2011 at 11:54Hi, This is already given to you with PSDexpress. Firstly, go to Project > Preference and enable the ABEL equation editing capability. A new option will be given in the main design flow diagram - Edit / Add Logic state...
Posted on May 17, 2011 at 11:54Hi, This enables port A as peripheral IO. Port A then looks like the internal data bus at the selected addresses. Pages 11 and 12 of AN1560 detail this quite clearly This is available http://www.stmcu.com/files/mcu/897...