2009-06-10 04:21 AM
2004-12-12 01:02 AM
Hi,
I have got a problem with the communication between the ST7538P and the PIC16F877. Everytime the first bit of the message which was received by the SPI Device is lost. Example: message: 10101010 (spi_write(0b10101010);) receiv. message: 01010100 My configurations are: ST7538P: carrier protection with conditioning PIC: SPI_Slave, SS disabled, CKP = 1, CKE = 0, SMP = 0 How knows the problem?2004-12-22 05:47 AM
Hi,
I am using PIC also, but I never used SPI, I have full control over the communication, it was made only in software. This is possible because the speed (baud rate) of the St7538 chip is slow enought. I know this does not help, but at least you know that there is someone somewhere in Brasil that makes the chip works. :-D Rafael Krapf BRASIL2009-06-10 04:21 AM
Hi Mr krapf,
I want to interface ST7538 with PIC 18F4550 microcontroller, but I don't know where to start. Could you please send me your source code? My email is: kamejoko80@yahoo.com