2004-03-30 07:39 AM
problem in programming through JTAG
2011-05-17 02:59 AM
hello,
I am using the uPSD323X from last one year. But for the first time i could see that the chip already programmed through JTAG ( more that 5 times)is not getting reprogram/erase. It's not able to communicate through JTAG . but the previous loaded image is working fine IT SHOWS: MISMATCH OF IDCODE here is the attached log file generated PLZ help Purvi2011-05-17 02:59 AM
hello,
i have not changed the user code from the default FFFFFFFF value. regards purvi2011-05-17 02:59 AM
Purvi,
I've seen this message if I accidentally have the wrong uPSD product selected in the JTAG programming screen within PSDExpress. For instance, if I was trying to program a uPSD3254A and I had selected the PSD854 as the device in the JTAG operation dialog box, it will show this error. Maybe take a look at this dialog (or your .jcf file if you're using it from the command line) and make sure it matches. Best Regards, Phaze426